A speedy messenger
that uses sound
for important notices.
Buzzers

LIBRARY
#11
Profile
- Beep beep! Boop! I’m the part that makes sounds.
- Machines need me to send signals.
- Buzzers can only make set sounds. Speakers can change sounds, but they’re a whole other part.
The Power of Buzzers
The tricky one who sends signals with sound.
Buzzers are used in electrical devices, automobiles, and other familiar machines.
For example, the sounds from buttons, washing machines, and thermometers all tell us things.
Sometimes loud noises warn us of bad things.

The Secret of the Power of Buzzers
Piezoelectric ceramic makes the noises!
The secret part of a buzzer that makes the noise is the “piezoelectric ceramic” inside it.
This is the part that vibrates when electricity flows through it. They make sound by making the air move when they do.

Friends of Buzzers

Various shapes of buzzers
Some buzzers are square, and others are round. They are made to fit the place where they will be used!
Trivia
What are the symbol and unit for buzzers?
The unit for S.P.L. is “dB” (for “decibels”). The more dB, the louder the sound.
For frequency, the symbol is “Hz” (for “hertz”). The more Hz, the higher pitch the sound.
Humans can hear sounds in the range of 40 Hz to 20 kHz (kHz stands for kilohertz, a unit of 1000 Hz).
QUESTION
Number three was right, guitar sounds and piano sounds!
You need speakers to change the tone!
Find the Buzzer!