A wonderful conductor
that keeps everything
moving smoothly.
Crystal Units

LIBRARY
#10
Profile
- I have a crystal inside me, like my name says!
- My powers let me send signals without messing up!
The Power of Crystal Units
The “heart” of the machine that keeps its rhythm.
Crystal units have the power to send signals with good rhythm. If you think of a machine like a person’s body, the crystal unit is the heart.
Just like when the heart pumps blood to your body, the crystal unit keeps rhythm for the signals it sends.

The Secret of the Power of Crystal Units
Crystals vibrate when they get electricity.
Crystal units have a crystal inside. It vibrates with an exact rhythm when it gets electricity. This rhythm controls when signals are sent.
Crystals aren’t just pretty gems, they have neat powers too!

Friends of Crystal Units

Ceramic Resonators
Crystal units are a type of “oscillator”. Other types can be made from piezoelectric ceramics.
Trivia
What are the units?
For smartphone crystal units, it’s about 10 MHz. That’s 10 million times each second!
Crystal units are also used in watches!
QUESTION
All machines need good rhythm.
Find the Crystal Unit!